Skip to main content

Kollmorgen Support Network

PC and KAS UDP communication: C# example (Visual Studio Express 2013) >

This example shows how to exchange data between a PCMM or AKD PDMM and a PC using UDP. The attached KAS program works with the target controller and 2 AKD drives.  The PC-based program is written in C# and receives the axis positions…

PC Connection Cables >

AKD The AKD Drives are connected to the PC or to a Hub or Switch via a standard Cat. 5 Ethernet cable.
Subscribe to PC