Skip to main content

Kollmorgen Support Network

Convert AKD-B Parameter File to AKD-P >

Instructions to convert a saved AKD-B parameter file into an AKD-P file to load into an AKD-P drive.

Procedures For Uploading and Downloading Drive Parameters With The S300 Drive >

Often users need to upload the parameters out of a failed drive and recommission a spare drive with the archived parameters. The attached documents detail these procedures. Note the documents assume you have the same model, hardware and firmware…

How to Transfer Parameters From One S600 To Another S600 >

A typical need is to transfer parameter settings from one drive to its replacement/spare.This could be from a file that is already archived or there may be a need to upload the parameters from the original drive to file first and then connect to the…

VLIMN Parameter (S300-S700) >

ASCII - Command VLIMN    

MVANGLB Parameter (S300-S700) >

ASCII - Command MVANGLB    

TEMPMFILT Parameter (S300-S700) >

ASCII - Command TEMPMFILT    

DICONT Parameter (S300-S700) >

ASCII - Command DICONT     Syntax Transmit DICONT     Syntax Receive DICONT <Data>  

DI2T Parameter (S300-S700) >

ASCII - Command DI2T     Syntax Transmit DI2T [Data]     Syntax Receive DI2T <Data>  

MI2T Parameter (S300-S700) >

ASCII - Command MI2T     Syntax Transmit MI2T     Syntax Receive MI2T <Data>  
Subscribe to parameters