Skip to main content

Kollmorgen Support Network

OS Prompt and EtherCat with AKD >

Hello, Could you confirm me that the object 1026.01 and 1026.02 could be mapped ? (On the EtherCat manual, it seems not, but on the xml description, it seems Yes) Moreover, it seems that as soon as I write a value in the 1026.01, the AKD panel…
Subscribe to OS Prompt and EtherCat