Back to top

The minimum ambient operating temperature, for the KBM, KBMS, TBM, and TBMS series motors is -40 degrees C.

The temperature rating of material is another item typically determined by the environment. Each material type has its own limitations for operating temperature range. The actual rating is defined as the allowable conductor temperature the insulation can safely withstand.