Back to top

Valid for S400, S600

Function

For controlling several servo amplifiers, start the communication with the first amplifier via RS232 and all other amplifiers via the CAN bus. Presumption for that is, that the CAN baud rates are identical and the station addresses of the servo amplifiers are set to different numbers.

Settings

Command

 Description