Back to top

Valid for AKD-T (AKD BASIC)

LED-akd.jpg

The standard AKD Fault Messages are valid for AKD BASIC as well. In case of a built-in I/O option board with SD card device, the errors described in Fault Messages I-O Option might occur as well.

Valid for AKD

Operation of the SD card device built into the I/O option board may occur in some Errors. These errors are displayed in the two digit AKD LED display. The coding is E followed by four digits. The errors are shown twice in the display, They are not permanently displayed.

Valid for AKD-B, AKD-P, AKD-T, AKD-M

The two digits LED display on the front panel of the drive shows the number of the fault or warning that occurred.

LED-akd.jpg

The left side of the LED displays "F" for a fault or "n" for warning.

Valid for AKD

The AKD Drives have a 2 digit display on the front. Status, faults and warnings are shown there.

Examples:

Valid for AKD-M (AKD PDMM)

The AKD PDMM Drives have a two digit plus a one digit display on the front. Status, faults and warnings are shown there.