Skip to main content

Kollmorgen Support Network

Building Power Supply Groups >

Since the failure rate of the servo amplifiers is very small, a line protection is sufficient from cost perspective. Further cost saving can be reached by group protection concept. If however a selective protection of the power supply is required…

S700, S300, S600, and S400 F24 Fault Code >

The F24 fault is created by the WMASK feature which allows a defined Warning (nX warning) to generate a fault message (defined by WMASK)

How to Recover from the Firmware or the PLC Marco Program Locking Up the S700 Servo Drive  >

How to Recover from the Firmware or the PLC Marco Program Locking Up the S700 Servo Drive

How to Recover from the Firmware or the PLC Marco Program Locking Up the S600 Servo Drive  >

How to Recover from the Firmware or the PLC Marco Program Locking Up the S600 Servo Drive

S700 with Dual STO Circuits >

If your S700 has two (2) STO safety circuits (drive P/N will be S7xxy2, where "xx" is the continuous current rating), please note: 1. Use the correct Installation Manual.  There is one (1) manual for the single channel STO and another for the…

How to Query S300 and S700 Current Faults  >

There are two parameters that can be used to query the S300 or the S700 drive's faults: ERRCODE or STATUS.  

CD Series 5 C9 Extended IO Connector >

There were some discrepancies in the old literature with pinouts and no details as to a mating connector. The PDF clarifies these details.

Linear Encoder Supported by AKD, S700, and S300 >

List of known linear encoder supported by AKD / S700 / S300.

Commissioning of Unknown Hall Motors with the S300 >

Commissioning of Unknown Hall Motors with the S300 Find out the hall counting direction  HALLDIR          MPOLES 0       Set no. of motor poles to 0        …
Subscribe to Lag