Skip to main content

Kollmorgen Support Network

Error with bit StatusWord.11 = Internal Limit Active. What happens? >

Dear community, We are having a big problem with a drive which is having a random error which stops the movement of the axis. As said, it is random, meaning that it sometimes appears and other times, the position control motion can be…
Subscribe to Internal Limit Active