Back to top
File Description 
Installation manual for AKD, AKD BASIC, and AKD PDMM drives. Describes the AKD series of digital drives and includes mechanical, electrical, and software installation information needed to safely install AKD.
Language 
English
Release 
1.20
Release Date 
Wednesday, November 11, 2020
File Description 
This manual provides information for the safe installation and setup of the PCMM Motion Controller. Includes general information, safety, handling, setup, troubleshooting, mechanical and electrical data. This release includes a Chinese section and miscellaneous updates.
Language 
Chinese, Simplified
English
French
German
Italian
Portuguese, Brazil
Russian
Spanish
Release 
D
Release Date 
Wednesday, September 4, 2019
File Description 
This manual describes the digital servo amplifiers of the Servostar 400 series.
Language 
English
Release 
11/2018
Release Date 
Monday, November 5, 2018
File Description 
This manual provides information for the safe installation and setup of the PCMM Motion Controller. Includes general information, safety, handling, setup, troubleshooting, mechanical and electrical data.
Language 
English
French
German
Italian
Portuguese, Brazil
Russian
Spanish
Release 
Release Date 
Tuesday, February 6, 2018

Note the firmware file referenced in this article can be found at the bottom or here: FW CDA-07

Make sure that the computer IP address is in the same range as the AKI-CDA Panel and that the subnet mask is the same. The computer will need to be set with a static IP address. If you need to set it as static or change the IP address you can do it through the Network Properties:

image

Firmware on an AKI-CDB Panel can be loaded either by Ethernet or by USB.

Setup if Loading via Ethernet 

If loading via Ethernet, make sure that the computer IP address is in the same range as the AKI - CDB Panel and that the subnet mask is the same.  The computer will need to be set with a static IP address.  If you need to set it as static or change the IP address you can do it through the Network Properties:

image

File Description 
S200 base unit quick start guide.
Language 
English
Release 
A
Release Date 
Friday, February 24, 2017

Installation information for Torquer Motors

After the motor and winding designation have been selected, the motor design should be incorporated in the layout phase of the mechanical design. A frameless brushless type motor may be either totally frameless, framed with an armature adapter machined to fit the customer’s existing shaft, or partially housed with a mounting flange or tabs for mounting the stator. 

File Description 
Installation manual for AKD, AKD BASIC, and AKD PDMM drives. Describes the AKD series of digital drives and includes mechanical, electrical, and software installation information needed to safely install AKD.
Language 
English
Release 
1.13
Release Date 
Wednesday, September 9, 2015