Skip to main content

Kollmorgen Support Network

Permanent Magnet Servomotor and Induction Motor Considerations >

Motion long considered a mainstay of induction motors, encroachment in the area of 50 hp and greater have been seen recently for some applications by permanent magnet (PM) servomotors.  These applications usually have dynamic considerations that…

VSTART Parameter (S300-S700) >

ASCII - Command VSTART     Syntax Transmit VSTART [Data]     Syntax Receive

MCOSPHI Parameter (S300-S700) >

ASCII - Command MCOSPHI     Syntax Transmit MCOSPHI [Data]     Syntax Receive MCOSPHI <Data>  

MVR Parameter (S300-S700) >

ASCII - Command MVR     Syntax Transmit MVR [Data]     Syntax Receive MVR <Data>  

MUR Parameter (S300-S700) >

ASCII - Command MUR     Syntax Transmit MUR [Data]     Syntax Receive MUR <Data>  

MFR Parameter (S300-S700) >

ASCII - Command MFR     Syntax Transmit MFR [Data]     Syntax Receive MFR <Data>  
Subscribe to induction motor