Skip to main content

Kollmorgen Support Network

Operating Induction Machines (S300-S700) >

To enable the servo amplifier to also operate induction machines with the exact speed, the control structure had to be extended. For the additional elements, you must adjust the corresponding parameters. In all sensorless modes, the output…

Sensorless >

Motors can be controlled without feedback by our servo amplifiers. Different control procedures are used for induction machines and synchronous motors: Sensorless Control for Induction Machines with S300-S700 Sensorless Control for Synchronous…
Subscribe to induction machines