Skip to main content

Kollmorgen Support Network

Inductance Range of the P7000 Stepper drive >

The P7000 was designed primarily for high inductance motors.  The AC model has two ranges of inductance based on bus voltage, and the DC model has its own inductance range. AC power (P70360): 160VDC bus - optimal motor inductance…

Motor Inductance >

Valid for S300, S400, S600, S700
Subscribe to inductance