Skip to main content

Kollmorgen Support Network

IL.KP by Modbus TCP >

For an application, I need to change IL.KP through Modbus TCP. The problem is that this register (address 454) is a 16-bit one, so I could not write a value > 65.535. Is there any solution to write a value bigger than 65.535 ? Best regards.
Subscribe to IL.KP through Modbus