Skip to main content

Kollmorgen Support Network

Legacy CD CP31010 Best Resource for Support >

I am trying to put together a machine using: (2) Goldline Xt motors MT1506B1-E2C1 & (2) ServoStar CD, CE03260-000000  I would like to find someone that would be able to help if I get stuck getting it going. If this is…

Using the Downloads Tool >

Table of Contents Overview Using the Downloads Tool The Results List Table of Contents1 - Overview

About Comments and Answers >

Comments may be made on articles in the Knowledge Base, as well as to Discussions, Feature Requests, and Questions in the Community. These are plain text messages meant to aid discussion. Answers are applicable only to Questions in the Community.…

Questions, Discussions, and Feature Requests >

In the Community page you'll find links to "Ask a Question", "Start a Discussion", and "Propose a Feature". This topic discusses the purpose and differences between them.

What is the purpose and scope of KDN? >

Purpose KDN is here for you; to help you learn, and to foster communication. KDN is used to communicate with Kollmorgen resources as well as other users.

How To Use KDN >

This is a collection of instructions and procedures for using KDN. It is an on-going project and is updated regularly. Knowledge Base Versus Community One of the most important things to understand is the difference between the Knowledge Base and…

Abbreviations >

Abbreviation English Area AF Fuse, fast Drive AGND Analog ground General AL Application Layer: the protocol that directly used by the process entities.   AM Fuse, medium Drive AT Fuse,…
Subscribe to help