The S700 ASCII MTIME parameter maximum is 600 seconds while many of the goldline motors have a much longer thermal time constant. Our application uses a M-607-B motor with a 38 minute (2280 sec) TCT on an S772 amplifier.
What's the…
S700 and S300 Series Drive Connections for the Incremental Encoder Feedback Goldline Series Motors
This article describes the Goldline motors' incremental encoder feedback connections and Goldline motors' power connections to the S700 and the S300.
AKD Series Drive Connections for Incremental Encoder Feedback Goldline Series Motors
This article describes Goldline motors incremental encoder feedback connections, Goldline motor power connections for the AKD drive.
Goldline Motors’ Encoder…
This article describes Goldline motors resolver feedback connections, Goldline motor power connections, AKD resolver feedback parameter values, and AKD Motor.Phase values.
AKD Series Drive Connections for the Goldline Series Motors Rev. J…
how would I go about finding the wire gauge size of the power wires of a Goldline motor (EB-106-A-11) with flying leads? I have looked in the Goldline motor catalog where just about all other information is listed except this. I…
how would I go about finding the wire gauge size of the power wires of a Goldline motor (EB-106-A-11) with flying leads? I have looked in the Goldline motor catalog where just about all other information is listed except this. I…
Hello,
Do you guys have Goldline motor files to be downloads onto an AKD (AKD-B01206-NBAN-0000)? Here is the goldline part number: B-404-B-B3
We are wondering if you have the parameter files?