The following outlines setting up KAS project to read S700 Digital Inputs into a PxMM program:
Through high speed , deterministic PDO channel:
Use S700 FW 5.18 or greater
Set DRVCNFG3 Bit 16 = 1
November 4, 2016
AKD Firmware 1.15.0.1
Objective:
We, Kollmorgen, supply an AKD.XML file to be used with the EtherCAT CoE Master. It has one default configuration, “Interpolated Position”. Many Customers want to use different configurations from…
The status of the Ethercat/motion Engine can be monitored with the MLMotionStatus function block. http://kdn.kollmorgen.com/webhelp/kas/#11.TechRefs/MLMotionStatus.htm?Highlight=MLMotion
In a Project with the PLCopen Motion Engine, if the Ethercat…
In the IDE project , the way to read/write an AKD analog or digital IO is to first link a variable in the dictionary to the I/O point as follows:
- Go to the AKD drive item in the EtherCAT section of the project tree. Double click on the…