Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

stephens105's picture
stephens105
1 week 5 days ago
Troubleshooting EMI Noise and making EMC Compliance with Kollmorgen Drives.
Kollmorgen Support's picture
Kollmorgen Support
1 month 1 week ago
Choosing a controller that matches your project is important. You don't want to overspend on a device that is significantly more powerful than you need, but buying something that is not robust enough can be even more costly. By defining your project's number of axes, the desired cycle time (µs), and the complexity of the application, we can recommend the minimum viable controller that is best suited to your KAS project.
Joe Parks's picture
Joe Parks
1 month 1 week ago
Video embedded below shows how to use the Recipe feature built into KVB software to change the value of multiple tags all at once. You can create the recipe ahead of time through spreadsheet views in KVB software, or create new/modify existing recipes on the HMI panel.
jcoleman02's picture
jcoleman02
1 month 2 weeks ago

The 0x0688 or 0x0288 or 0x0289 fault is displayed on the keypad as an Undefined Fault. This fault code will be at the bottom of the keypad display. When connected to the ServoTuner software, these come up as Commutation Sensor Fault errors.

This fault is related to the commutation hall effect sensors in the encoder of the motor, and the corresponding wiring in the feedback cable.