Back to top

Many servo applications exist in which it is more practical to use a DC power supply for the motor bus power instead of using AC power.  Some of these include the use of batteries, generators, low voltage DC power supplies, and there are cases where high voltage DC power supplies are used just because of preference or availability.

The following applies to the AKD-x003y through AKD-x024y, where y = 6 or 7 (All AKD drives except for the AKD48).