Skip to main content

Kollmorgen Support Network

Trio Motion Controller Modbus TCP Communications to AKD1G >

This application note demonstrates configuration and addressing for Modbus TCP communications using a Trio Motion Controller to AKD1G. The application notes is an example only and the implementation and verification of proper operation of the…

Choosing a KAS Controller >

Choosing a controller that matches your project is important. You don't want to overspend on a device that is significantly more powerful than you need, but buying something that is not robust enough can be even more costly. By defining your…

Wiring Pin-Out For AKM with Commutating Encoder to B8000 Series Drives >

This document contains pin-out information for the AKM1x and AKM2x C connectors with commutating encoder to the B8000 series of IDC drives.

Tuning Rotary Direct Drives >

Valid for S400, S600
Subscribe to Controller