Skip to main content

Kollmorgen Support Network

Hiperface DSL >

HIPERFACE® DSL (Sick AG) is equivalent to the two-wire RS485 standard with a transmission rate of 9.375 MBaud. The data transmission is synchron to the servo amplifier clock, which can be up to 11.95 microseconds short.

ProfiNet >

General PROFINET ( Pro cess Fi eld Net work) is the Profibus & Profinet International (PI) open industrial Ethernet standard for automation. There are two types Profinet types, Profinet CBA and Profinet IO:

DeviceNet Bus >

 DeviceNet is a CAN based field bus which is used mainly in the automation engineering. Number of nodes Maximum 64 nodes per bus segment. Node addresses (0 to 63) can be set with DIP switches on the servo amplifiers. Baudrate Selectable…

SERCOS Bus >

General SERCOS (SErial Real time COmmunication System) interface is a worldwide standardized digital interface  for the communication between controls and drives (IEC 61491 and EN 61491).
Subscribe to communication protocol