Skip to main content

Kollmorgen Support Network

AKD2G Certifications >

  Safety CCC CE UL UR cUL cUR EAC RoHS10 REACH WEEE AKD2G MV STO IEC 61508-1/-2, IEC 61800-5-2, IEC 62061,  ISO…

EAC Marking >

EAC is the abbreviation for Eurasian Conformity. The mark is used in the states of the customs union (Russia, Belarus, Kazakhstan) similar to the European CE mark. A manufacturer or supplier, who adds this mark to his product, declares
Subscribe to certifications