This article is related Cam Build & Release Organization.
The attached file consists of a FB you may use in your project. In some machines, we need different cam profiles and we change these profiles for system…
Series of three videos showing how to add camming to a PLCopen project in the KAS IDE with a PDMM or PCMM controller. The first video shows how to use the cam creation tool in the KAS IDE to create a cam profile by specifying master and slave points.…
This is an example of switching a cam profile from a 5th order polynomial profile to a parabolic curve. The program contains the code needed to switch the cam profile on the fly from a polynomial motion curve to a parabolic (constant acceleration)…
Attached is a demo program that contains two subprograms to import data from a file on a PDMM SD card, or export data from an array to the SD card. This data can then be used to build a cam profile in the program and update the motion on the…
Camming in AKD-Basic
Camming is a method of making a slave AKD-T drive follow a master encoder signal (or a virtual master) in a non-linear fashion. It is very similar to electronic gearing, except that the slave does not have to match the…
Attached is a demo program showing an example of how to use cam creation function blocks to build a completely new profile while a program is running. The main function required is MLProfileBuild located in the function block library under…