Back to top

The following link points to an example from the KAS Online Help which discusses process data transferred to the Bus Coupler for variable mapping.

Analog I/O Parameters - I/O Terminals for Variable Mapping

The DC bus link, or connections, of the AKD drive can be used to connect the DC bus of one drive to the DC bus of another drive.  The connection is done in parallel between two or more drives, with the maximum number of drives being limited by the total sum of the current ratings, as specified in the drive manual.   This method is commonly used to help maintain the DC bus voltage within the allowable range in applications involving motor regenerative power (regen).  As a motor is back-driven (driven by the load, gravity, external forces, etc.), the motor produces po