Skip to main content

Kollmorgen Support Network

Brakes activation by noise?? >

Hello community, We have a AKM23D motor. We are monitoring the +-24V brake signal, which seems to have a lot of noise and we think that this could be the cause of a random stop of the motor. As you can see in the following figure, the stop of…

Enquiry for - Electromagnetically Released Linear Brake >

Hi Team , we are looking for ‘Electromagnetically Released Linear Brake’. We are currently using product from Ortlinghaus having part number ‘0-801-000-10-002-000’. We understand from Ortlinghaus that they have stopped manufacturing these products…

Brake Enabled without line voltage. >

A customer is wondering how quickly the AKD can enable the brake on the motor without line voltage. Considering the 24VDC bus voltage is still operating the STO. Imagine somebody goes inside the electrical panel where the AKD will be housed…
Subscribe to brakes