Back to top
Hello, I have a question, I am programming the AKD KOmorgen with the Python script and want to program an autotuning with the AKD
Unfortunately, I couldn't find any commands for autotuning in the user manual, but only for manual
Could you please tell me what are the command for autotuning
Thanks you very much
Kind regards
Tom



Tips and Tricks for the AKD Performance Servo Tuner (Autotuner and Bode Tool)

 

Increase the Excitation Current

If the excitation current is too low, the motor will not be able to move enough to measure a good frequency response.  If the autotuner fails to complete because of not moving enough, then increase the excitation current.  Set the excitation level to “Manual” and enter a higher current amplitude.

Taking a bode plot in Workbench for AKD tuning analysis.

 

1.  Put the drive in Torque mode

2.  Leave the excitation level set to “Automatic”

3.  Set the Performance Servo Tuner mode to “Bode Plot”

4.  Set the measurement to “Plant”

image

 

5.  Select Plot

In the Plots tab, select “Plot Plant”, and uncheck all other boxes.

How to use the Performance Servo Tuner to de-tune the AKD