Back to top
File Description 
AKD2G Servo Drive Firmware for CANopen, EtherCAT, EtherNet/IP, PROFINET, and Analog devices. This firmware complies with recently revised U.S. and E.U. export regulations (E.U. Dual-Use Regulation 428/2009, and U.S. Dual-use regulation EAR Category 3 under ECCN3A225).
Language 
English
Release 
02.08.00.000
Release Date 
Friday, October 22, 2021

The following link points to an example from the KAS Online Help which discusses process data transferred to the Bus Coupler for variable mapping.

Analog I/O Parameters - I/O Terminals for Variable Mapping

When using torque mode in an AKD Basic program, you must set DRV.CMDSOURCE=0 (Service) and DRV.OPMODE = 0 (Torque) in the program.

If the program executes an IL.CMDU command while DRV.CMDSOURCE=5, it will throw an F825 Runtime error. The runtime error message says that DRV.CMDSOURCE must be set to 5. This is normal for position control, but for torque control it must be set to zero. The Basic program will continue to run even after the command source changes to Service mode.

Valid for S300, S600, S700

Application (example)

For an auger the packaging quantity is to be adjusted by a motion task and the control is to be realized simply and user-friendly . The quantity can vary in a defined +/- range.

Realization

With a digital input the motion task is started, the motion task selection is done with a framing potentiometer due to the necessary voltage levels.