When sending/receiving data remotely using Modbus TCP, what should the minimum time delay (in milliseconds) be between each register read for the AKD, in
I am getting a F402 with resolver feedback on an akm. I can clear this error but whenever I enable the error comes back. I have done a continuity test and compared this with another drive and motor combination we have…
I'm using an AKD 306 in a simple camera track setup. Foot pedals provide +- 10v for velocity setpoint. We set software limits as endstops.
When the camera reaches a limit it causes an n107/n108 Fault and the system decelerates at cs.dec (1000…
The following utility provides a connection between AKD servo drive (other than the Profinet drive) and Siemens SIMATIC S7-1200/S7-1500 programmable logic controllers (PLC) using Modbus TCP programmed in TIA V13.
The application contains the…
Can anyone suggest the safest way to ensure that a slave axis is always following it's master? Both axes are identical linear actuators being controlled by AKD drives in position mode. For example:
1) if the slave drive is disabled, the…
Are there any tutorials or videos showing how to create and set-up a custom motion profile table with AKD - AKD Workbench? The AKD Workbench help-file has good detail on "Motion Profile Table" and "Motion Profile Table Advanced" but an…