Hello, I'm Jaehyung Kim, a Ph.D. candidate in South Korea.
Currently, I am working on building a system that incorporates the Kollmorgen workbench, AKD-P00307, and AKMH24D-CCK2R Motor. However, I am facing an issue related to the VBus.
The…
On the AKD2G the 'All paramters' node under Device setinngs tree has been removed.
Is this deliberate or is it a bug or missing implementation?
It is still available on normal AKD drives.
/Jørgen
I had message like attached photo during connection between driver (AKD-P00607-NBCC-D000) and PC.
Why does it happen this message? What I do for solving this problem?
Please, give me your advice.
I can't see some information on Workbench since I changed laptop. OS is Windows10 (Japanese) . What is the root cause? Please see following screenshots.
Hi!
When Workbench 1.17.0.2215 finds the drive it crashes every time. The local network is behind a Moxa router.
I have two network connections, one directly to the router and one on the outside of the router (WAN).
If both are on Broadcast mode…
I have an AKD-P00306-NBCC-E000 driving a Tecnotion TM3 linear syncronous motor, I am trying to tune the drive but when I press 'Start' it runs through the Positive and Negative friction tests, then fails with the following error. I…
Debugging interaction problem between WorkBench and drives may be facilitated by using the built-in logging mechanism.
Where are the application and the log files in your system:
The easiest way to access the application or the log files is to open…
Hello,
We encountered a little problem with AKD Workbench when we go on Feedback1 window.
With some laptops, we have a popup window indicated an error (see the attached jpeg). It is not a big issue as, if we choose Continue, it works fine.
I…