Skip to main content

Kollmorgen Support Network

KAS PLCopen Teach Home for absolute feedback devices >

This article and attached sample KAS project show how to use PLCopen function blocks to teach a position so that an axis with an absolute feedback device will not need to run a home routine to move to a sensor or hard stop each time you power…

BiSS >

The bidirectional digital sensor interface (BiSS) safeguards the communication between position encoder and servo amplifier and can transfer measurements of up to 8 sensors simultaneously. For 1 to 8 participants the interface master delivers the…
Subscribe to Absolute Encoder