Skip to main content

Kollmorgen Support Network

AKD EtherCAT and CANopen Landing Page >

This landing page contains links to other articles and downloads relating to AKD EtherCAT and CANopen communication.

TwinCAT 3 To AKD2G EtherCAT Setup and Demonstration >

The attached video covers important topics such as ESI (XML) file acquisition and importation into TwinCAT 3. Basic setup and motion from the TwinCAT 3 console are also demonstrated. Finally how to recognize and resolve a mismatch…

Setup of EtherCAT master to run an AKD2G in DS402: Profile Velocity Mode >

Help setup the AKD2G in DS402 Profile Velocity mode.  This document assumes the EtherCAT Master has “free mapping” function available. The ability to select what data is to be shard every update cycle. This information may not make sense to you…

Setup of EtherCAT master to run an AKD2G in “DS402: Cyclic Synchronous Position Mode” >

AKD2G Firmware AKD2G_01-90-13-000 Objective: We, Kollmorgen, supply an AKD2G XML files to be used with the EtherCAT CoE Master.  It has one default configuration, “cyclic Synchronous Position” mode.  Many Customers want to use EtherCAT…
Subscribe to TwinCAT