Kollmorgen Corporation (“Kollmorgen”) declares that the AKD2G drives have memory devices as shown in the table below. The non-volatile memory that may contain user settings and data may be cleared as indicated.
Summary of Juran's Mean Time Between Failure (MTBF) for AKD & AKM. Data up through 2014.
Purpose
A rough calculation of the Mean Time Between Failure (MTBF) based on historical data. This tool is to be used at a customer's request. MTBF is not…
The AKD Installation Manual, the S700 (S701-S724) Installation Manual, and the S700 (S748-S772) Installation Manual all show a vibration specification as "CLASS 3M1 According To IEC60721-3-3".
To further clarify, the following information is…