Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

Joe Parks's picture
Joe Parks
2 weeks 1 day ago

The video embedded below goes through how to add security features with Kollmorgen Visualization Builder (KVB). Shows how to create accounts with different levels of security and how to make objects in HMI screens either hidden or disabled unless you login to a certain level of security

kenny.hampton@kollmorgen.com's picture
3 weeks 5 days ago
This article explains how to unlock an S600 when it boots up with an 8.8.8 on the display, or locks up while downloading firmware.
cwontrop's picture
cwontrop
1 month 1 week ago

This article contains an application note on using AKD2G within a KAS environment. It will help you when developing a KAS application which includes AKD2G drives. 

A future version of this article will include the text, and not just the application note in PDF form.

didier.kuttel's picture
didier.kuttel
2 months 3 days ago

WorkBench (version ≥ 2.2.2.4811) has some accessible parameters to tweak the way data are exchanged with the drive. Keywords sent to the drive and answers returned will be grouped together to build bigger packets of data. This is particularly helpful on networks with high latency. It is also useful for slowing down the polling interval to avoid overloading the communication channel on slower networks.