Back to top

Setting clock time (RTC) PCMM

0 votes
+ vote
Vote up!
How can I tune real time clock of PCMM?
0 Comments

1 Answer

0 votes
+ vote
Vote up!

Hello Konstantin, 
PCMM han no real time clock. You can set the time by PLC but after next reboot it will be lost as referred in the manual.

 

Comments

Hey! Thanks for the answer.
It doesn't matter to me that the time will be reset after a reboot.
I need to set the time on PCMM after connecting to it via UDP.
But I can only GET the timestamp from the PLC, not set.
Is it possible to SET clock time?

Krounis - Sun, 07/04/2021 - 20:01

Hello
There are some "get" functions for the rtc, but no write, so you could use these for initialisation and then write your own UDFB. In the past this has been achieved easily by using our AKI2G and using modbus tcp writing the rtc information from the AKI2G to the Pxmm.

I Gibb - Mon, 07/19/2021 - 11:18
Log in or register to post comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.