Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

Set the Date and Time from the Internet on a PDMM | 10 Jan 2018 | |

Set the Date and Time from the Internet on a PDMM

Can anyone tell me how to programmatically set the date and time from the internet (or a local NTP server) on a PDMM?

Thanks,

Sam

Comments & Answers

C Wontrop said ...

C Wontrop | Fri, 01/12/2018 - 20:53

The PxMM platform does not have an internal real time clock. Time information can be sent to the PxMM via one of the supported network interfaces: Modbus TCP/IP, ProfiNET, Ethernet I/P, UDP or HTTP. It can also be brought into the PxMM via a connection to a remote shared directory. If an AKI HMI terminal is being used in the application, it can also send time to the PxMM through Modbus TCP/IP

Here are links to more information:

http://curvegen.kollmorgen.com/webhelp/kas/#8.AdvancedTopics/Motion Bus and Fieldbuses.htm%3FTocPath%3DAdvanced%2520Topics%7CMotion%2520Bus%2520and%2520Fieldbuses%7C_____0

http://curvegen.kollmorgen.com/webhelp/kas/#13.Troubleshoot/Connect_Rem…

http://curvegen.kollmorgen.com/webhelp/kas/#11.TechRefs/SharedDirPathCo…
ref:_00D80TfnV._5008017Duqa:ref

Will Gaffga | Fri, 01/12/2018 - 22:12

Carroll's answer is correct, though the first link is broken. Try this:
http://curvegen.kollmorgen.com/webhelp/kas/#8.AdvancedTopics/Motion%252…

About this Question

Sam Dickinson
Taxonomy: