Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

toddevans01's picture
toddevans01
2 days 13 hours ago

NOTE: This landing page is under construction and a work in progress.

             Check for more content and application notes in the near future.

 

Command Type 0x08-Velocity Setpoint Example

 

 

jcoleman02's picture
jcoleman02
1 week 5 days ago
This article contains a list of differences between AKD2G and AKD1G related to Profinet.
jcoleman02's picture
jcoleman02
2 weeks 2 days ago

The AKD command source (DRV.CMDSOURCE) is set automatically by the EtherCAT/CANopen master controller.  There is no need to set this in Workbench when using the fieldbus.  And there is no need to read DRV.CMDSOURCE to verify that it's set correctly as long as there is nothing configured in the drive that would change it, such as a digital input.  Set the fieldbus mode of operation with object 6060h and let that automatically set the correct command source.

jcoleman02's picture
jcoleman02
3 weeks 1 day ago

EoE Overview

EoE = Ethernet over EtherCAT

This allows communication between Workbench (installed on the EtherCAT master PC) and the AKD using Telnet communication over the EtherCAT network.  It allows connecting to the drive with Workbench without needing a separate PC or Ethernet port.

Types of Connections

EoE connection: