Back to top

Restart Problem

0 votes
+ vote
Vote up!

Hi, when I do an interrupt and I restart my program, the value I enterred in an integer from the HMI get set to 0 everytime.  Is there a was to keep the value while still using the restart function?

I have an AKD-T00306-ICAN-0000 and a AKI2G-CDA-MOD-05T-000

0 Comments

2 Answers

1 vote
+ vote
Vote up!

Maybe it helps to define the integer variables in AKD Basic as non-volatile variables, even if you will not execute a power cycle. 

Refer to AKD WB online help >> AKD Basic Statements > DIM << for more details
http://curvegen.kollmorgen.com/webhelp/workbench/English

0 Comments

0 votes
+ vote
Vote up!
Thank you!
0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.