Back to top

Question about Browse catalog on Stepper optimizer

0 votes
+ vote
Vote up!

Dear team, 

I have 2 questions for Browse catalog on Stepper optimizer.

1) Regarding temperature curve, if a graph is over the limit, Can’t i use the  product?

2) How many percentage of variation tolerance of pullout torque?

Thank you in advance,

Best Regards,

Kurata

0 Comments

1 Answer

0 votes
+ vote
Vote up!

Per Case 01759133:

Hi Kurata,
Per your questions (below), if the blue performance line of the motor exceeds the orange temperature line on the graph, then the motor will overheat in continuous operation. If you need continuous operation, try selecting a solution (if available) that appears in green.

Pull-Out torque of a stepper motor is a function of both the drive and frequency. It’s more of a system-level question, which is why we don’t publish it. We do publish the holding torque, however. Depending on the model/series, the associate catalog should have a tolerance on the holding torque. For example, on the PMX line, the holding torque values are assuming +/-10%.

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.