Back to top

Project restore / load from web browser

It would be nice to be able to restore / load a project to a PDMM / PCMM without having to use a SD card. 

Comments

cwontrop's picture
cwontrop
Marc, thank you for the suggestion. It will be forwarded to our Marketing/Engineering teams. There is one alternative to note.  In a situation in which a kas project needs to be sent to a customer  to be installed in a PxMM controller, it could be saved by the sender  to the SD card via the KAS web server connected to a PxMM. The SD card then removed from the PxMM  and plugged into a PC SD card reader. The  files then  transferred to the PC and  sent to the user. The user can then transfer the files to the SD card, then insert the SD card into the PDMM  and load using the PxMM front face buttons.