Back to top

Problem with Input Mapping on a PDMM

0 votes
+ vote
Vote up!

I have a problem with inputs on PDMM :

When I go to the AKD configuration, I see that the input is working fine :

image

 

But the variable I map to this input is always off ...

image

I use FW 1.17.00.004 for the AKD and version 3.00 for the KAS ...

I don't remember to have such problem with version before..

Best regards.

 

0 Comments

2 Answers

0 votes
+ vote
Vote up!

Thanks a lot,

I have found the problem : as I need just a small program to handle I/O of the PDMM, I have not initialize the Motion Engine... So obviously, the mapping of the I/O does not work !!! By running Motion Engine, no problem, everything works fine.

Regards.

0 Comments

0 votes
+ vote
Vote up!
As a test, please created a new variable in the IDE dictionary and map to X7 pin10. Is the problem still there? IF not, then it looks like the IxT1 is somehow being force low elsewhere in the project.
0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.