Back to top

Problem with Electronic gearing settings

0 votes
+ vote
Vote up!

Hi every one,

First, thank you for those who will take some time to answer my questions. I'm trying to build a system that has two servos, one as a leader, and one as a slave (electronic gearing). I succeed only half of it as the slave follows the master in only one direction. My problem is that i can't find the setting that force the slave to follow the master in either direction. Could some one tell me which setting i have to change to fulfill my requirements?

thank you

hervéPS: i have an old version of the S300 (5.86 and a 3.75 firmware version for my two servos) and a 3.1.1 version of driveGUI

0 Comments

1 Answer

0 votes
+ vote
Vote up!

Hello,

I have never ran into an issue that only let electronic gearing  work in one direction.  Can you send me your S300 drive's parameter file?

[email protected]

Thanks,

Kenny Hampton

 

 

 

 

 

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.