Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

Old Smartdrive | 11 Oct 2017 | |

Old Smartdrive

Hi!! 

I am working whit a old drive: SmartDrive. I installed MotionLink for SmartDrive but I need a TL file to configure motor parameters. 

The motor is a GOLDLINE BRUSHLESS; model: B-106-A-31-R3. 

Could you send me the file, or give me information about where I can download. 

Thanks!! 

Comments & Answers

Paul Coughlin said ...

Paul Coughlin |

Attached is the Catalog Data Sheet containing the motor parameters.

These motor parameters may be entered into the SmartDrive via the MotionLink software.

kenny.hampton@… said ...

kenny.hampton@… |

The motor's  parameter file can be loaded from the Smart Drive Software "GUI".  You are required to select the B-106-A motor in the GUI software.

This is a link to Smart Drive Software:

http://www.kollmorgen.com/en-us/products/drives/discontinued/discontinued-drives/

Scroll down to the header Smart Drive (KOL) and the software file is listed as  (Smart Drive Software Rev.1)

Daniel Barradas | Mon, 10/30/2017 - 21:33

Thanks for your replay!
I have the model D03001 of the SmartDrive, I have a doubt regarding the connection of the DC Bus + and the DC Bus -.

What do I have to connect to these terminals?

About this Question

Daniel Barradas
Taxonomy: