Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

motor power through slip ring | 03 Feb 2016 | |

motor power through slip ring

Hello!

I need a motor to work on rotating platform and this motor is controlled by S346 - 400V. Motor and S346 are on different sides of slip ring (see attach).

So i cut power cable (DE-107473) near motor end  and made like this:

- 4 wires from slip ring fixed side (of 200mm length) come to X9 connector

- 4 wires of slip ring moving side (of 200mm length) connect by screw terminals with 4 wires of power cable I cut

- connector comes to motor

Feedback cable is standard; S346 is controlled by CANopen from PC. 

 When I start program, it works OK for only one second, I see motor position changed a little. Then comes Error F023 (CAN bus fault) and motor stops. Also S346 stops responding by CAN

How do I solve this problem? With another power cable (uncut DE-107473) motor rotates fine and stable until I stop it. 

Thanks for help

Comments & Answers

jcoleman02 said ...

jcoleman02 | Wed, 02/03/2016 - 14:43

The F23 fault is related to the CANopen communication.  It is not related to the motor power cable, except that an unshielded motor power cable will output a lot of EMI.  The EMI can cause communication problems.  If the CANopen communication works fine on the same system when not using the slip ring, then I would guess that the problem is due to the slip ring not providing shielding.

iakovlev said ...

iakovlev | Thu, 02/04/2016 - 04:48

thanks! 

problem was in handmade CAN-cable. Made it shorter and better quality and all works

About this Question

iakovlev
Taxonomy: