Back to top

MMC cant connect with picpro

0 votes
+ vote
Vote up!
I have had several MMC smart drives fail
I can't connect with picpro but the drive shows up when I ping the address

Whats causing the drive not to connect to picpro when its pinging back?
 
0 Comments

1 Answer

0 votes
+ vote
Vote up!

It is recommended to acquire a serial PicPro cable ( DB9 to mini-din ) for troubleshooting.

It was also determined that the version of PicPro used was v16 and the Windows OS attempted was Window7 or Windows 10.

PicPro 16 has never been tested for these OS ( it was tested with Vista ) so the recommendation is to use PicPro 18 ( latest ) and to update

the firmware in the Digital MMC smartdrives and the Drive Resident control cards and migrate the program to the PicPro 18 environment moving forward.

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.