Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

Max. Torque in Velocity mode | 06 Feb 2023 | |

Max. Torque in Velocity mode

Hello,

I have the following situation.

A Servodrive is connected with CANbus to the controller, the drive is connected to a motor which that drives a belt.

Now I want to set the speed and max. torque that of the motor during operation.

What is the best mode to use velocity or torque?

And how can I control both (speed and torque) in one of these modes?

 

 

Comments & Answers

Michael Stingl said ...

Michael Stingl | Wed, 02/08/2023 - 14:02

 

Hello,

please look at the ASCII-Comand: ICMDVLIM

jcoleman02 said ...

jcoleman02 | Mon, 02/27/2023 - 19:51
If you want to command velocity via CANbus and have the drive limit torque to a preset maximum, then use IPEAKP and IPEAKN to limit the peak (maximum) current.

I Gibb | Tue, 02/07/2023 - 11:59

Parameter IL.VLIMIT has been added to the AKD firmware to limit motor velocity while operating in torque mode. Setting it to a non-zero value will limit the velocity - in torque mode only - to the range of -IL.VLIMIT to IL.VLIMIT. The parameter IL.VLIMIT was released in firmware 01-14-04-00 beta on April 16, 2016

BennyB | Tue, 02/07/2023 - 12:06

I have a S300 does it have the same parameter?

About this Question

BennyB