Back to top

Mapping variables to I/O and PDO with a structure as a variable type

It would be very nice to be able to map a variable that has a custom structure data type to a PDO or I/O point.  The variable in the structure would obviously still have the same required data type (bool, int, etc.) but wouldn't require the user to mess up their variable scheme by creating an additional variable just for mapping.

Comments

Joe Parks's picture
Joe Parks
Thank you for the feedback. I have entered an enhancement request in our issue tracking system to relay the information to our software development team. I agree, it would be nice to be able to map an element of a structure directly instead of having to create an extra variable to act as a middle man