Back to top

Kollmorgen EP Series PMDC Motor IP Rating

0 votes
+ vote
Vote up!

Hi All

Could you please help me figure out the IP rating of the following motor and more specifically to what extent would the motor be protected against water ingress?

Name: 1/3 HP, 24 Volt - 1750RPM (SRC Rated NEMA Standards - Explosion Proof)

Model No: EP3624-2757-7-56BC-CU

Product Code: FGE0245

 

Thank You

image

0 Comments

2 Answers

0 votes
+ vote
Vote up!

Thanks. It is imperative that we do get an IP rating for the motor. So would how do we go about figuring that out?

Could you direct me to the person/department I should reach out to with info about about the application and the environment the motor is being used/exposed in? 

0 Comments

0 votes
+ vote
Vote up!

Per the PMDC Design Engineer:

" This is an explosion proof motor.  AS such, we don’t assign it an IP rating.  It is not for use in environments that are wet.  If the customer has specific questions we can address this in a case, provided all details re: the environment and application."

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.