Skip to main content

Kollmorgen Support Network

CNC PPCO CNC PPC da Kollmorgen é um sistema de comando numérico computadorizado desenvolvido no Brasil que possui diversas funcionalidades e comunicação EtherCAT com os servo-acionamentos AKD e ABD da Kollmorgen.
Rodrigo Gallo Rodrigo Gallo
March 23, 2023 Portuguese, Brazil
KAS IDE fails to load ESI files and display missing ESI files error messages when FIPS security policy is enabledKAS IDE fails to load the ESI files from the ESI library and fails to add the EtherCAT devices to the project when the FIPS (Federal Information Process Standards) security policy is enabled on the computer.
Prashanth Morishetty
March 6, 2023 English
Trade ComplianceKollmorgen is committed to sourcing components and materials from companies that share our values regarding respect for human rights, integrity and environmental responsibility.
Bethany Seymour Bethany Seymour
February 21, 2023 English
AKT and AKT2G Remote I/O ComparisonThe AKT2G family is recommended for new applications requiring remote I/O in a PCMM or PDMM KAS application. This article and attachment compares the AKT2G Remote I/O family with the AKT Remote I/O family.
C Wontrop C Wontrop
February 8, 2023 English
(ABM)(3D Drawings) Altra Brasil Servo SeriesThese 3D models are intended to guide your design activities and can be used as reference information. Be sure to consult a Kollmorgen expert to ensure you have the most current and accurate information for critical aspects of the design work.
Leonardo Souza Leonardo Souza
January 18, 2023 English
(ABD & ABM) Altra Brasil Servo SeriesThe Altra Brasil Servo Series, consisting of the ABD® (Altra Brasil Drive) and ABM® (Altra Brasil Motor) series, is a complete line of EtherCAT-based servo drives developed specifically for the Brazilian market.
Leonardo Souza Leonardo Souza
January 18, 2023 English
Convert AKD-B Parameter File to AKD-PInstructions to convert a saved AKD-B parameter file into an AKD-P file to load into an AKD-P drive.
jcoleman02 jcoleman02
January 10, 2023 English
AKD2G Profinet PNU Reads and Writes Application Note Revision AThis application note demonstrates AKD2G parameter access from a S7-1500 PLC using the SinaPara function block for multi-parameter access and the SinaParaS for single parameter access.
toddevans01 toddevans01
January 4, 2023 English
KAS IDE v4.00 is now available!!New Features Next Generation Controller Software Compatible with PCMM/PDMM (1st Generation Controllers) 64-bit Runtime (2nd Generation Controllers) AKD2G Modular Device Profile (MDP) I/O MDP IO support for model variants<
Prashanth Morishetty
December 14, 2022 English