S300 & S700 Errors and WarningsThis content is extracted from the DriveGUI documentation. |
Will Gaffga |
English | |
Configuration of PLC Siemens S7-1500 ProfiNetTM and Kollmorgen AKD®2G-SPPThis is a guide to configure the PROFINET IRT communication in between the CPU S7-15xxTx-PN and the AKD2G-SPP PROFINET. The result is to manage both axes by means of the Technology Objects that the PLC provides. The axes will be configured in Velocity Mode and the PLC will handle the position loop… |
Stefano Giacomelli |
English | |
Speedtec Cable Notice (O-Ring)Remove AKM motor connector O-ring for use with Speedtec cable connectors. |
jcoleman02 |
English | |
AKD2G Gantry Application SetupA gantry system consists of two motors sharing a load with minimal wasted energy used in opposing each other. This document is an attempt to help with setup and use of the Kollmorgen gantry control embedded in the AKD2G two-axis drive. For the scope of this document, I will refer to the two axes… |
Will Hulbert |
English | |
Value Line Cable Update NoticeKollmorgen is excited to announce our new Value Line cable offering! |
Will Hulbert |
English | |
Coupler Sizing - AKT2G Remote IOThe AKD-PDMM controller/drive, PCMM standalone controller, AKD, AKD2G, and S700 drives all contain hardware I/O that can be used in an application to interface to other control elements on the machine. Typically, to minimize overall system cost, IO point on these products are used first before the… |
C Wontrop |
English | |
AKD EtherNet/IP to Omron PLCsAKD Ethernet/IP and Omron |
toddevans01 |
English | |
Configuring BBH SCU with AKD2G SRA parameters This article shows how to make a simple safety Application with KAS and SafePLC2. The Functional Safety parameters can be configured in WorkBench or in the BBH SafePLC2. Both methods are described here. |
jeeva |
English | |
AKM2G Standard Voltage and Low Voltage Winding Thermal Sensor OptionsA description of the thermal sensor options for the AKM2G Standard and Low Voltage series motors. | English |
Don't know if you need a servo or stepper?
Unlocking Design Possibilities with Frameless Motors
Read More