Skip to main content

Kollmorgen Support Network

S-Curve Corner Transition – Design and CalculationsThe reason the S-Curve Corner Transition was designed was due to the existing Corner Distance Transition having a discontinuity in the acceleration vector when entering the circular arc of the transition.
Will Gaffga
English
CNC PPC - Registradores especiais do CNCLista de registradores especiais do CNC para acessar dados em tempo real, status do CNC e comandos.
Will Gaffga
Portuguese, Brazil
Retrofit KAS EtherCAT Backups with AKD2G FirmwareThe AKD2G drives with firmware versions 02-12-00-001 (and later) do not support downgrading the firmware to the versions 02-12-00-000 (or earlier). The KAS EtherCAT backups created using AKD2G firmware 02-12-00-000 (or earlier) are not capable of restoring the drive’s configuration once any AKD2G…
Jeanie
English
AKD2G EtherCAT W7011 Warning and F7011 Fault Synchronization Error SupportThis article provides details related to cause and remedy of the W7011 warning and F7011 Fault in the AKD2G EtherCAT drive.
toddevans01
English
Using Siemens PD_TEL9_DrivePos with Telegram 9 for Positioning with AKD2G Profinet RTThis document provides test results when using Siemens PD_TEL9_DrivePos function block with AKD2G Profinet Telegram 9
Will Gaffga
English
KAS v4.01 Software is now available!! KAS v4.01 Software is now available!!
dusty.schafer
English
AKD and AKD2G Resolver Excitation Output Voltage Specification AKD and AKD2G Resolver Excitation Output Voltage Specification
Will Gaffga
English
AKD1G Reading Faults Over Ethernet IPDiscussion on methods for reading faults over Ethernet IP.
toddevans01
English
AKD2G Controlled Stop and Holding Brake TimingThis is an explanation of the controlled stop and brake timing functionality in the AKD2G drive.
Will Gaffga
English