KAS IDE Motor Setup Wizard
Dear All,
Previously I use KAS IDE 3.02.080765 to setup motor parameter using Motor Setup Wizard under configuration mode. Recently i download the KAS IDE 3.07.086841, the motor setup wizard button gray out. Any condition to enable the motor setup wizard button?
Thanks
Comments & Answers
Will Gaffga said ...
Hi. It has been determined that this is a bug (#11156) that will be fixed in a future release. When the bug is fixed it will be noted in the KAS Release Notes, which can be seen in each release's PDF or in the help.
Apologies for the inconvenience, but thank you for helping us continually improve our software.
Hi. An answer is being
Hi. An answer is being investigated.